Fiber Optic Cable Length Source

IMPORTANT: This domain is required because it tells the length autoupdater the field from which the applicable length data should be pulled for a cable or segment.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Code

Description

FOOTSTAMPS

Footstamps

DOCUMENTS / FIELD NOTES

Documents / Field Notes

GIS LENGTH + SLACK LOOP LENGTH

GIS Length + Slack Loop Length

OTDR LENGTH

OTDR Length

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?