Fiber Circuit Channel

TIP: This domain is not required but helps assign a name to a wavelength. For example, CHAN03 could be assigned to 1330 MHz. Additionally, this domain makes populating circuit types faster and less error prone since users pick the coded value from a drop-down list versus typing it.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

CHAN01

CHAN01

CHAN02

CHAN02

CHAN03

CHAN03

CHAN04

CHAN04

CHAN05

CHAN05

CHAN06

CHAN06

CHAN07

CHAN07

CHAN08

CHAN08

CHAN09

CHAN09

CHAN10

CHAN10

CHAN11

CHAN11

CHAN12

CHAN12

CHAN13

CHAN13

CHAN14

CHAN14

CHAN15

CHAN15

CHAN16

CHAN16

CHAN17

CHAN17

CHAN18

CHAN18

CHAN19

CHAN19

CHAN20

CHAN20

CHAN21

CHAN21

CHAN22

CHAN22

CHAN23

CHAN23

CHAN24

CHAN24

CHAN25

CHAN25

CHAN26

CHAN26

CHAN27

CHAN27

CHAN28

CHAN28

CHAN29

CHAN29

CHAN30

CHAN30

CHAN31

CHAN31

CHAN32

CHAN32

CHAN33

CHAN33

CHAN34

CHAN34

CHAN35

CHAN35

CHAN36

CHAN36

CHAN37

CHAN37

CHAN38

CHAN38

CHAN39

CHAN39

CHAN40

CHAN40

Other

Other

Unknown

Unknown

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?