Fiber Connection Location

TIP: This domain is not required but designates if the connection is on the front side or the back side of the equipment.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Backside

Back Side

Frontside

Front Side

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?