F_BACKSIDEPORT
-
ObjectID fields are automatically created (by Esri) when you create the schema.
-
GlobalID fields are required by Fiber Manager and are created with Esri's Add Global ID tool (Manage > Add Global IDs).
-
Tables must be versioned for an SDE database. See Esri’s documentation for more information about versioning tables.
-
Tables must also be converted to ArcFM Objects.
-
In ArcGIS applications, there are four numeric data types: Short Integer, Long Integer, Float, and Double. The choices reflect a balance between minimizing storage space while still allowing enough range and precision for the field to be useful. For example, because lengths typically have decimals, these fields are assigned either Float or Double.
In the table below, any field set to integer does need to be either a Short or Long Integer, as these fields cannot contain decimals. So, the decision comes down to the minimum and maximum values you need for the field:
-
Short Integer Storable Range: -32,768 to 32,767
-
Long Integer Storable Range: -2,147,483,648 to 2,147,483,647
So, as an example, would you ever have more than 32,767 patch panels on a single rack? No. So, the RackPosition field could be a Short Integer. Conversely, foot or meter stamps along a cable could easily exceed 32,767. So, CableMarking fields should be a Long Integer. Our integer recommendations err on the side of more range and usefulness, but your company could decide to change a Long Integer to a Short Integer (or a Double down to a Float) if you knew the maximum values would never exceed the types’ upper threshold.
-
Alias: Backside Port
Field |
Data Type |
Default Value |
Domain |
Length/Precision |
---|---|---|---|---|
DefaultHeight Alias: Height |
Short Integer |
1 |
||
DefaultWidth Alias: Width |
Short Integer |
1 |
||
FiberChildClassModelName Alias: Fiber Child Class Model Name |
Text |
50 |
||
FiberParent Alias: Fiber Parent |
Guid |
|||
FiberParentClassModelName Alias: Fiber Parent Class Model Name |
Text |
50 |
||
GlobalID Alias: Global ID |
Guid |
|||
ImpliedConnectionSourceGuid Alias: Implied Connection Source Guid |
Guid |
|||
PortName Alias: Name |
Text |
50 |
||
PortNumber Alias: Number |
Short Integer |
|||
PortPositionOnCard Alias: Position on Card |
Short Integer |
|||
PortType Alias: Type |
Text |
Fiber Port Type |
50 |
|
RackSides Alias: Sides |
Text |
Fiber Connection Location |
50 |
|
ThisFiberClassModelName Alias: This Fiber Class Model Name |
Text |
PatchPanelBacksidePort |
50 |
Field Display
Primary Display Field: Choose this field in the ArcFM Properties Manager. The chosen field is displayed when using ArcFM tools such as the ArcFM Locator and ArcFM Attribute Editor. Your company can choose the most useful field to display for the end users. If the chosen field is null for the selected or identified features, the display field defaults to the ObjectID.
Because this choice also determines what is displayed on the Patch Panel Connection Report and Circuit Trace Report, PortName is recommended.
Model Names
FIBERCIRCUITPARTICIPANT, FIBERCONNECTABLEOBJECT,FIBERGRIDABLEOBJECT, FIBERIMPLIEDCONNECTIONDESTINATION, FIBEROBJECT, PATCHPANELBACKSIDEPORT, SUPPORTSALOSS, SUPPORTSBLOSS, SUPPORTSCONNECTIONTYPE, SUPPORTSDISCONNECTWARNING, SUPPORTSSELFCONNECTION
Field Model Names
DefaultHeight: FIBERGRIDDEFAULTHEIGHT
DefaultWidth: FIBERGRIDDEFAULTWIDTH
FiberChildClassModelName: FIBERCHILDCLASSMODELNAME
FiberParent: FIBERPARENT
FiberParentClassModelName: FIBERPARENTCLASSMODELNAME
GlobalID: GLOBALID
ImpliedConnectionSourceGuid: FIBERIMPLIEDCONNECTIONSOURCEGUID
PortName: FIBERCIRCUITREPORTFIELD
PortNumber: FIBERCONNECTIONDISPLAYSORTFIELD, FIBERIMPLIEDALIGNMENT, PORTNUMBER
PortPositionOnCard: FIBERGRIDPOSITION
PortType: PORTTYPE
RackSides: FIBERFACETSCONTAINEDBY
ThisFiberClassModelName: THISFIBERCLASSMODELNAME
Object AutoUpdaters
On Feature Delete: ArcFM Fiber Object Deleted
Field Autoupdaters
ChangeDate — On Feature Update: ArcFM Current Date
ChangeUser — On Feature Update: ArcFM Login User Name
CreationDate — On Feature Create: ArcFM Current Date
CreationUser — On Feature Create: ArcFM Login User Name