Import Sample Schema and Properties

If you do not already have the Fiber Manager schema in your geodatabase, you can import it from the Minerville sample geodatabase. This option helps you import not only the schema, but also the model names, domains, properties, and autoupdater assignments. If you use this process, the default values and aliases are also set up automatically.

This set of subtopics start with an empty geodatabase, and end with a configured geodatabase using the standard data model. While this “clean path” approach might not exactly match your implementation, the steps are illustrative and demonstrate the benefits of exporting and importing the settings and properties.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?