Operational Maps

Operational maps contain the GIS features that users interact with in ArcFM Mobile. The Operational Maps tab shows all your existing maps and provides a way to add new ones.

Take it for a drive! (The link opens/switches to the Solution Center app, accesses the Operational Maps tab, and initiates a new operational map.)

Follow these steps to add a new operational map:

  1. Click the Add New button.

  2. Type a display name, which is required.

  3. Provide a URL to a map service, which is also required, and click Save. You are notified if the URL isn’t to a valid map service.

After creating a new operational map, you can configure replicas, searches, markups, tracing, and outbound messages, if those are applicable.

Users can access this operational map only if they are members of a Portal for ArcGIS group that has access to the underlying feature service.

At least one Portal Administrator must log in to ArcFM Solution Center at least one time after any changes are made to group-based map access in Portal for ArcGIS, before ArcFM Mobile users can see these changes.

TIP: Troubleshooting: If a map service is down, you may not be able to perform certain functions against it. When you see Down as the status, this could mean one of three things:
  • The map service is not currently running on the ArcGIS Server or cannot be contacted due to a networking issue. Double-check that the URL to the service is correct.

  • If your organization uses Portal for ArcGIS/AGOL to secure your map services, the map service may require you to be logged in as a Portal for ArcGIS/AGOL user. Ensure that you are logged in as a Portal for ArcGIS/AGOL user with permissions to access the map service.

  • The service is just unavailable at the moment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?