Searches

Publishes in Mobile config and Solution Center

Solution Center
By adding and configuring searches, you help eliminate the need for users to select multiple feature layers when performing a common search. Doing so also provides the flexibility of searching on any fields in the designated feature layer; whereas with the default search, only the Display Field for each layer is searched. For example, you may configure a search on the Fuse, Dynamic Protective Devices, and Switch feature layers, called Protected Devices, specifying multiple different search fields for each. Users then need only select that configured search and provide their search criteria. ArcFM Mobile does the rest, constructing the appropriate database query based on the configuration.

Publishes in both
TIP: When the status of a map is Down, the Create button is greyed out.

Publishes in both
  1. Click Create and type a descriptive Display Name, which is required, that clearly identifies the action of the search.

  2. To add a feature to your search, click Add New Searchable Feature.

  3. Select a feature from the popup window. You have to include at least one feature.

  4. Click Apply.

  5. For each feature that you add, click the Edit button.

  6. In the Edit Fields popup, click the fields you want in the search.

    The fields you select are populated under the feature.

  7. When that’s finished, click the Save button that is now enabled.

Publishes in both
IMPORTANT: As soon as one search is configured for an operational map, the default search functionality is replaced with configured searches. Default behavior returns if all configured searches are removed.

Edit or Delete a Search

Use the:

  • Delete button to remove a search from the operational map.

  • Edit button to change the display name, and/or change the configured features and fields.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?