ArcFM Connectivity Evaluator (ACE)
The ArcFM Connectivity Evaluator (ACE) is a separate application from Solution Center. Its core function is to test and verify connectivity to ArcFM services and, depending on the application, connectivity to Azure Service Bus. This is a crucial prerequisite prior to performing Solution Center configuration or any XI series app configuration, given that you need connectivity for the configuration to work.
IMPORTANT: Schneider Electric is continuously making changes to increase the reliability and
resilience of our services. Our development teams have introduced
features that allow automatic failover services for all primary services.
We are leveraging Azure features called Application
Gateway and Traffic Manager to enable every customer
to have a primary and secondary region. This requires a
minor change to firewall rules on your side plus coordination
with our Operations team. To read more about this change, refer
tp the App Gateway article on myArcFM.
|
Access the ACE Installer
The ACE installer can be downloaded via the ArcFM Solution Center article on myArcFM.
Because the ACE tool is testing connectivity, it only works after your company’s tenant is created.
The ACE tool can be run as many times as needed until all issues are corrected. This is particularly true throughout the implementation process.
Verify Core Outbound URL Access
Verifying access to the core outbound URLs is extremely helpful during the very early stages of your implementation. This verification includes the ability to access core ArcFM Services, Auth0, and the Tenancy service itself. Access to these core services is a prerequisite for essentially any other configuration or implementation step.
To verify access, follow these steps:
-
Launch the ACE tool.
IMPORTANT: Verifying core outbound URL access can happen on any machine. The ACE tool does not necessarily need to be installed on the same machine that contains the actual XI series application. To check core outbound URLs, you only need the ACE tool and tenant ID. To verify access to other services and the Azure Service Bus, the ACE tool needs to be installed on the same machine as the actual application. -
If this is the first time you have launched the tool, “Please enter your organization’s name” then click Submit.
-
To check core outbound URLs, you do not need to log in. Refer to the Firewall Rules for Ports topic for more information.
-
Click the View <tenantName> Allowlist button.
-
The interface displays icons for the specific services and for All Services.
-
To see all the required URLs for all services, click All Services.
-
Click Open Services Report to generate a PDF of service URLs. This is a great way to share the URLs that require allowlisting.
-
To test access to the actual URLs, click the desired service icon (for example, the Login Info icon).
-
You can test services individually, or click the Test All icon to start the process (the URLs in the following image are just examples and your URLs differ).
After running a test, the application displays the test results along with an HTTP status code.
The following table includes a description of the possible result codes, whose standard descriptions are taken from the protocols established by the Internet Engineering Task Force (IETF):
Code
Result
Description
Troubleshooting
200
OK
The request has succeeded. The information returned with the response is dependent on the method used in the request
The server responded as expected. The service is functioning normally.
302
Found
The requested resource resides temporarily under a different Uniform Resource Identifier (URI). Since the redirection might be altered on occasion, the client should continue to use the Request-URI for future requests. This response is only cacheable if indicated by a Cache-Control or Expires header field.
Most likely a misconfigured service URL. Copy test results, contact support, and include copy of test results.
400
Bad Request
The request could not be understood by the server due to malformed syntax. The client should not repeat the request without modifications.
Problem with the ACE tool. Update to current version and try again.
401
Unauthorized
The request requires user authentication.
Problem with ACE tool not sending an appropriate authentication header. Update to current version and try again.
403
Forbidden
The server understood the request, but it is refusing to fulfill it.
Misconfigured service permissions. Make note of the service being tested. Copy test results, contact support, and include copy of test results.
404
Not Found
The server has not found anything matching the Request-URI. No indication is given of whether the condition is temporary or permanent.
Misconfigured service endpoint. The service has been removed, is down, or customer has not been configured for service. Copy test results, contact support, and include copy of test results.
407
Proxy Authentication Required
Indicates that the client must first authenticate itself with the proxy.
Customer has proxy in use and user must authenticate to proxy first before connecting to ArcFM services. Copy test results, contact support, and include copy of test results.
408
Request Timeout
The client did not produce a request within the time that the server was prepared to wait. The client may repeat the request without modifications at any later time.
Several possible causes: non-existent endpoint, customer proxy did not forward request to ArcFM services, etc. If error repeats upon re-try at a later time, copy test results, contact support, and include copy of test results.
500
Internal Server Error
The server encountered an unexpected condition which prevented it from fulfilling the request.
Problem with ArcFM service endpoint. Update to current version and try again. If error repeats, copy test results, contact support, and include copy of test results.
502
Bad Gateway
The server, while acting as a gateway or proxy, received an invalid response from the upstream server it accessed in attempting to fulfill the request.
Most likely caused by customer firewall or proxy. Could be a single endpoint or all. If a single endpoint, add the service endpoint URL to the firewall and/or proxy and try again. If error repeats, copy test results, contact support, and include copy of test results.
-
Optionally, click Open Test Report to generate a PDF version of the test results.
NOTE: Reports are saved in the directory C:\Users\user_name\AppData\Local\ArcFMConnectivityEvaluator\app-version#\Reports.
-
-
Verify Application-Specific Services and Connectivity to Azure Service Bus
Going a step further, after verifying core services, it is also critical to verify access to application-specific services and to the Azure Service Bus. Each XI series application provides details of the required connections and ports, and the ability to test the connections in bulk or individually. The ACE tool handles both core and application-specific services, but the key difference is that to check application-specific services, the ACE needs to be installed on the same machine hosting the app itself.
-
Install the ACE tool on the same machine that runs the XI series application you are testing. In other words, if you are testing connectivity for Designer XI, run the tool on the same machine where Designer XI is installed.
-
Launch the ACE tool.
-
If this is the first time you have launched the tool, “Please enter your organization’s name” then click Submit.
-
Log into your tenant. The login methods were established when your tenant was created, and your choices likely vary from the following image:
-
The interface displays icon for the various, application-specific services in addition to All Services.
-
As explained previously, All Services provides a view-only list of URLs.
-
Test connectivity to a service by clicking the desired service icon (for example, the Solution Center icon), then click the Test All icon to test access.
-
Optionally, click Open Test Report to generate a PDF version of the test results.
NOTE: Reports are saved in the directory C:\Users\user_name\AppData\Local\ArcFMConnectivityEvaluator\app-version#\Reports
Authenticate with the ACE Tool
In the event that you need to authenticate using the ACE tool, within the app select the appropriate tenant from the drop-down list:
After selecting a tenant and successfully authenticating, you can view the full application allowlist:
The ACE tool window provides two options: All Services and Login Info.
When you click All Services, you are provided with a full application allowlist, similar to the following image:
When you click Login Info, you are provided with a way to test all services that are required to log in. The tests need to be initiated on the machine that hosts any ArcFM XI series application.