Mobile Client Workflows

The Mobile Client subtab, or workflow family, is the home of client-side workflows specific to the Mobile application. Some examples are the Approve, Open, and Reject workflows. Think of these client-side workflows as actions an individual might take on their individual mobile device while working with the application.

Available Tools

The functions, tools, and subtabs are largely the same between the Studio and Default Workflow Studio tabs. However, the Studio tab provides a few additional tools on its subtabs.

The following buttons are available on all subtabs in Default Workflow Studio. Refer to the Studio topic to learn about its additional tools.

The Add New button creates a new workflow. We recommend not using this on the Default Workflow Studio tab as new workflows created here cannot be saved or published. This tab is only for Schneider Electric-provided workflows.
The Refresh button updates the list of workflows in the drop-down.
The Show Revision History button provides the revision history of the workflow.

Revision history of a workflow is recorded and can be helpful to track changes made to different versions of workflows over time. Refer to the Default Workflow Studio topic to read more about revision history records.

Below is an example of a Mobile Client workflow, the Approval — Approve workflow.

Mobile Client subtab of Default Workflow Studio displaying the Approval — Approve workflow

Workflow Properties

Property Definition

Name

The title of your workflow.

Minimum Client Version

The minimum version of Editor required to execute this autoupdater workflow. This field only applies to autoupdater workflows on the ArcGIS Server subtab. We recommend leaving this field blank on all other types of workflows.

Workflow Status

Published — the workflow is published and represents the latest version of the workflow.

Draft — the workflow is in draft form and not published.

Retired — the workflow has been replaced by a newer version and this version is retired and no longer published.

Example — this is a workflow example that is useful for copying and pasting into a new workflow as a template or starting point.

Workflow Metadata Id

The unique identifier on each version of a workflow that allows you to call a particular version.

Workflow Ancestral Id

This identifier designates the starting point of a workflow’s history, after which all versions maintain that Ancestral Id.

Version

The version number of the workflow. Useful in tracking the evolution of workflows as administrators make changes.

Updated By

The user name of the last person to modify the workflow. The OOTB workflows provided by Schneider Electric say Updated By Schneider Electric Team, or sometimes say none.

Updated On

The date the last workflow modifications were made.

Expression Language

The coding language that is used within the workflow.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?