Default Workflow Studio

The Default Workflow Studio contains the Schneider Electric-provided workflows. It is akin to a library of provided workflows for you to use as they are, or you can create copies of them in order to manipulate them to suit your company’s needs.

  • The Default Workflow Studio also comes with default test cases Schneider Electric has used to validate the provided workflows.

  • Every customer starts with the Designer Workflow. This workflow incorporates two core procedures: “Push to GIS,” and “Send for Approval.”

If you are ready to modify this default workflow, press the “Override in Tenant” button at the bottom of the interface. This toggles you to the Studio tab, and it creates a draft copy of the workflow from Default Workflow Studio.

IMPORTANT: The functions, tools, and subtabs are the same between the Studio and Default Workflow Studio tabs. For explanations of the tools, see the Studio topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?