Multiple Tenant Drop-Down

If you work with multiple tenants, use the drop-down to quickly change to a different tenant. This is much faster than signing out and signing back in to the different tenant. For example, you might have production and development tenants, especially during the implementation phase, and this is a quick way to toggle between the two configurations.

TIP: Production tenants are marked with the letter “P” as seen in the image above.

For this drop-down to appear, the following requirements must be met:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?