Operating the Circuit Breakers
Circuit Breaker Operating Control Accessories for General-Purpose Applications
The following table shows the operating control accessories compatible with the ComPact NSX DC circuit breakers for general-purpose applications. For more information, refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.
|
Operating Control Accessory |
NSX100 DC |
NSX160 DC |
NSX250 DC |
NSX400 DC |
NSX630 DC |
NSX1200 DC |
||||
|---|---|---|---|---|---|---|---|---|---|---|
|
1P |
2P |
3P/4P |
1P |
2P |
3P/4P |
3P/4P |
3P/4P |
3P/4P |
2P |
|
|
Toggle handle |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
Rotary handle |
– | – | ✔ | – | – | ✔ | ✔ | ✔ | ✔ | ✔ |
|
Motor mechanism |
– | – | ✔ | – | – | ✔ | ✔ | ✔ | ✔ | ✔ |
|
Communicating motor mechanism |
– | – | ✔ | – | – | ✔ | ✔ | ✔ | ✔ | ✔ |
Circuit Breaker Operating Control Accessories for Photovoltaic Applications
The following table shows the operating control accessories compatible with the ComPact NSX DC circuit breakers for photovoltaic applications. For more information, refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.
|
Operating Control Accessory |
NSX80 |
NSX100 |
NSX125 |
NSX160 |
NSX200 |
NSX400 |
NSX500 |
|---|---|---|---|---|---|---|---|
|
4P |
4P |
4P |
4P |
4P |
4P |
4P |
|
|
Toggle handle |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
Rotary handle |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
Motor mechanism |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
Communicating motor mechanism |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
Handle Position
The handle position indicates the state of the circuit breaker:
Remote Indication
Information is available remotely:
-
From the indication contacts
-
From the wireless indication auxiliaries
-
By using a communication network
These indication auxiliaries can be installed on site.
For more information about the remote indication and communication options, refer to the summary tables of auxiliaries.
Remote Electrical Stop Command
The remote electrical stop command can be given by electrical control
auxiliaries regardless of the control type in use.
To obtain a remote electrical stop command, use:
-
an MX shunt trip release, or
-
an MN undervoltage trip release, or
-
an MN undervoltage trip release with time-delay unit (the time-delay unit overcomes the problem of micro-cuts).
For more information about the electrical control auxiliaries, refer to the relevant topic.