Electric Auxiliary Devices Summary
Electric Auxiliary Devices for General-Purpose Applications
The following table shows the electric auxiliary devices that can be added to the ComPact NSX DC circuit breakers for general-purpose applications. For more information, refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.
|
Electric Auxiliary Device |
NSX100 DC |
NSX160 DC |
NSX250 DC |
NSX400 DC |
NSX630 DC |
NSX1200 DC |
||||
|---|---|---|---|---|---|---|---|---|---|---|
|
1P |
2P |
3P/4P |
1P |
2P |
3P/4P |
3P/4P |
3P/4P |
3P/4P |
2P |
|
|
OF or SD indication auxiliary (wired or wireless) |
– | ✔ | ✔ | – | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
SDE auxiliary contact |
– | – | ✔ | – | – | ✔ | ✔ | ✔ | ✔ | ✔ |
|
MN undervoltage trip release |
– | ✔ | ✔ | – | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
MX shunt trip release |
– | ✔ | ✔ | – | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
BSCM breaker status control module |
– | – | ✔ | – | – | ✔ | ✔ | ✔ | ✔ | ✔ |
|
NSX cord |
– | – | ✔ | – | – | ✔ | ✔ | ✔ | ✔ | ✔ |
Electric Auxiliary Devices for Photovoltaic Applications
The following table shows the electric auxiliary devices that can be added to the ComPact NSX DC circuit breakers for photovoltaic applications. For more information, refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.
|
Electric Auxiliary Device |
NSX80 |
NSX100 |
NSX125 |
NSX160 |
NSX200 |
NSX400 |
NSX500 |
|---|---|---|---|---|---|---|---|
|
4P |
4P |
4P |
4P |
4P |
4P |
4P |
|
|
OF or SD indication auxiliary (wired or wireless) |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
SDE auxiliary contact |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
MN undervoltage trip release |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
MX shunt trip release |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
BSCM breaker status control module |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
|
NSX cord |
✔ | ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
Electrical Auxiliaries Installation Demonstration Video
To access a demonstration video about the installation of electrical auxiliary devices in a ComPact NSX100-250 3P circuit breaker, click the following link: https://youtu.be/zDqRyZHBWr4, copy and paste the link to your Web browser, or scan the QR code.
Safety Instructions for Photovoltaic Applications
Special care is required when adding electric auxiliary devices into circuit breakers for photovoltaic applications.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK
Failure to follow these instructions will result in death or serious injury.
|
Slots for Electric Auxiliary Devices on ComPact NSX100/160 DC 2P Circuit Breakers
The following table shows the possible slots for electric auxiliary devices mounted in the case. Only one auxiliary can be installed per slot. For more information, refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.

|
Electric Auxiliary Device |
Slot |
||
|---|---|---|---|
|
A |
B |
C |
|
|
OF1 (wired or wireless) |
✔ | – | – |
|
SD (wired or wireless) |
– | ✔ | – |
|
MN |
– | – | ✔ |
|
MX |
– | – | ✔ |
Slots for Electric Auxiliary Devices on ComPact NSX100-250 DC 3P/4P Circuit Breakers
The following table shows the possible slots for the electric auxiliary devices mounted in the case. Only one auxiliary can be installed per slot. For more information, refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.

|
Electric Auxiliary Device |
Slot |
Comments |
||||
|---|---|---|---|---|---|---|
|
A |
B |
C |
D |
E |
||
|
Standard remote indication and control auxiliaries |
||||||
|
OF1 (wired or wireless) |
✔ | – | – | – | – |
For all trip unit types and control types (toggle handle, rotary handle, or motor mechanism). |
|
OF2 (wired or wireless) |
– | – | – | ✔ | – | |
|
SD (wired or wireless) |
– | ✔ | – | – | – | |
|
SDE (wired or wireless) |
– | – | ✔ | – | – | |
|
MN |
– | – | – | – | ✔ | |
|
MX |
– | – | – | – | ✔ | |
|
Communication |
||||||
|
BSCM |
– | – | ✔ | ✔ | – |
For sending OF, SDE (BSCM), and SD (NSX cord) data to the communication network. |
|
NSX cord |
– | ✔ | – | – | – | |
Slots for Electric Auxiliary Devices on ComPact NSX400–630–1200 DC 3P/4P Circuit Breakers
The following table shows the possible slots for the electric auxiliary devices mounted in the case. For more information, refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.

|
Electric Auxiliary Device |
Slot |
Comments |
||||||
|---|---|---|---|---|---|---|---|---|
|
A |
B |
C |
D |
E |
F |
G |
||
|
Standard remote indication and control auxiliaries |
||||||||
|
OF1 (wired or wireless) |
– | ✔ | – | – | – | – | ||
|
OF2 (wired or wireless) |
– | ✔ | – | – | – | – | – |
For all trip unit types and control types (toggle handle, rotary handle, or motor mechanism). |
|
OF3 (wired or wireless) |
✔ | – | – | – | – | – | – | |
|
OF4 (wired or wireless) |
– | – | – | – | – | – | ✔ | |
|
SD (wired or wireless) |
– | – | – | – | ✔ | – | – | |
|
SDE (wired or wireless) |
– | – | – | – | – | ✔ | – | |
|
MN |
– | – | – | ✔ | – | – | – | |
|
MX |
– | – | – | ✔ | – | – | – | |
|
Communication |
||||||||
|
BSCM |
– | – | – | – | – | ✔ | – |
For sending OF, SDE (BSCM), and SD (NSX cord) data to the communication network. |
|
NSX cord |
– | – | – | – | ✔ | – | – | |
Operation of the Indication Contacts
The following table shows the position of the indication contacts (or outputs) relative to the position of the actuator and main contacts.
The state of the NO contact is open:
-
for OF indication contacts when the circuit breaker is in the O (OFF) position.
-
for SD and SDE indication contacts when the associated function is not active.
Sequence chart of the OF indication contacts relative to the main contacts

A Main contacts
B Position of OF changeover contacts
Operation of the Wireless Indication Auxiliaries
The wireless indication auxiliary provides the same information as a standard wired indication contact in OF, SD, or SDE positions. The information is sent remotely to a gateway or panel server.
During commissioning of the wireless indication auxiliary, the user defines the type of information sent: Open/Close or Trip.


DANGER