Opening, Closing, and Resetting Circuit Breakers With Communicating Motor Mechanism
Introduction
Manage the communicating motor mechanism with the communication network.
For this function, it is necessary to:
-
Install a Breaker Status Control Module (BSCM) and the NSX cord.
-
Use a communicating motor mechanism.
Connect the BSCM to the network with by the NSX cord:
-
To receive closing, opening, and reset commands from the circuit breaker.
-
To transmit the circuit breaker states: O (OFF), I (ON), Tripped by SDE.
The BSCM can be configured using EcoStruxure Power Commission software.
The schematic for the communicating motor mechanism in the BSCM can be configured. It must be created in strict accordance with the simplified motor mechanism schematic.
CAUTION |
|---|
|
HAZARD OF REPEATED CLOSING ON ELECTRICAL FAULT
Do not modify the wiring diagrams for the motor mechanism.
Failure to follow these instructions can result in injury or equipment damage.
|
Manual Operation: Opening, Closing, and Resetting Locally
The process is the same as the standard motor mechanism.
Automatic Operation: Opening, Closing, and Resetting Remotely
The process is the same as the standard motor mechanism.
Resetting After a Trip on Electrical Fault
Without modifying the factory configuration, the process is the same as the standard motor mechanism.
Using EcoStruxure Power Commission software to reconfigure the BSCM module authorizes remote resetting after a trip on electrical fault on a circuit breaker with communicating motor mechanism.
CAUTION