TM-DC Thermal-Magnetic Trip Unit for 2P Circuit Breakers from 630 A to 1200 A
Introduction
The TM-DC thermal-magnetic trip unit for 2P circuit breakers from 630 A to 1200 A are built-in trip units.
They are designed for DC general-purpose applications.
The TM-DC 2P trip units provide:
-
adjustable thermal threshold
-
adjustable magnetic pick-up
Description
Setting the Thermal Protection
The thermal protection pick-up Ir is set by a 4-setting dial.
Turning the thermal protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pick-up Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.
|
Trip Unit Rating In (A) at 40 °C (104 °F) |
|||
|---|---|---|---|
|
630 |
800 |
1000 |
1200 |
|
Pick-up Ir (A) at 40 °C (104 °F) |
|||
|
441 |
560 |
700 |
840 |
|
504 |
640 |
800 |
960 |
|
567 |
720 |
900 |
1080 |
|
630 |
800 |
1000 |
1200 |
Setting the Magnetic Protection
The magnetic protection pick-up cannot be adjusted and equals the value shown below:
|
Trip Unit Rating In (A) |
|||
|---|---|---|---|
|
630 |
800 |
1000 |
1200 |
|
Pick-up Ii (A) +/– 20% |
|||
|
1575 |
2000 |
2500 |
3000 |
|
1890 |
2400 |
3000 |
3600 |
|
2205 |
2800 |
3500 |
4200 |
|
2520 |
3200 |
4000 |
4800 |
|
2835 |
3600 |
4500 |
5400 |
|
3150 |
4000 |
5000 |
6000 |