DOCA0066EN-05

Locking the Circuit Breaker

Locking Accessories

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
When the circuit breaker toggle handle is locked in the (O) OFF position, always use a properly rated voltage sensing device to confirm that power is off before working on equipment.
Failure to follow these instructions will result in death or serious injury.

Use locking accessories to lock the toggle handle in the I (ON) or O (OFF) position.

Accessory

Padlocks

Accessory that is part of the case

Use up to 3 padlocks (not supplied) 5–8 mm (0.2–0.3 in) in diameter

Accessory that is detachable

Use up to 3 padlocks (not supplied) 5–8 mm (0.2–0.3 in) in diameter

NOTE: Locking the toggle handle in the I (ON) position does not disable the circuit breaker protection functions. If there is an electrical fault, the circuit breaker trips without altering its performance. When unlocked, the toggle handle moves to the Trip position. To return the circuit breaker to service, refer to how to open, close, and reset the circuit breaker.

Sealing Accessories

Use sealing accessories to prevent circuit breaker operations.

Seal

Prohibited operations

Escutcheon mounting screw

  • Dismantling the escutcheon

  • Accessing the auxiliaries

  • Dismantling the trip unit

Transparent protective cover

  • Altering trip unit settings

  • Accessing the test port for the trip units

Mounting screw for terminal shields

Accessing the power connection (protection against direct contact)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?