Plug-in Circuit Breaker
Introduction
Plug-in base circuit breakers make it possible to:
-
Extract and/or rapidly replace the circuit breaker without having to touch the connections on the base.
-
Allow for the addition of future circuits by installing bases that will be equipped with a circuit breaker at a later date.
-
Isolate the power circuits when the circuit breaker is mounted on or through a panel. It acts as a barrier for the connections of the plug-in base. Insulation is made complete by the mandatory short terminal shields on the circuit breaker.
The following types of circuit breaker can be installed in a plug-in base:
-
3P and 4P circuit breakers for general-purpose applications
-
Circuit breakers with toggle handle, direct rotary handle, or extended rotary handle
-
Motor-operated circuit breakers
The plug-in circuit breaker is made up of the fixed circuit breaker and a plug-in kit, which includes:
-
Plug-in base
-
Power connections
-
Short terminal shields
-
Safety trip interlock
For more information about plug-in circuit breaker installation, consult the instruction sheets on the Schneider Electric website:
-
GHD16276AA, Plug-in base for ComPact NSX100-250
-
GHD16316AA, Plug-in base for ComPact NSX400-630
Plug-in Kit and Chassis Installation Demonstration Video
To access a demonstration video about the installation of a plug-in kit and chassis for withdrawable ComPact NSX100-250 circuit breakers, click the following link: https://youtu.be/XaXO6QgeWvM, copy and paste the link to your Web browser, or scan the QR code.
Disconnecting the Circuit Breaker
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow this procedure to disconnect the circuit beaker:
|
Step |
Action |
|
|---|---|---|
|
1 |
Switch the circuit breaker to the O (OFF) position. |
|
|
2 |
Remove both mounting screws. |
|
|
3 |
Pull out the circuit breaker, keeping it horizontal. |
|
-
The auxiliary circuits automatically disconnect because of the connectors located on the base and at the rear of the circuit breaker.
-
Open the circuit breaker before disconnecting it. If the circuit breaker is in the closed I (ON) position when disconnecting, a pre-trip mechanism trips the circuit breaker before the pins are disconnected.
Connecting the Circuit Breaker
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow this procedure to connect the circuit beaker:
|
Step |
Action |
|
|---|---|---|
|
1 |
Switch the circuit breaker to the O (OFF) position. |
|
|
2 |
Connect the circuit breaker. |
|
|
3 |
Replace both mounting screws. Tighten the screws to a torque of 2.5 N•m (22.1 lb-in). |
|
-
The auxiliary circuits automatically disconnect because of the connectors located on the base and at the rear of the circuit breaker.
-
Open the circuit breaker before connecting it. If the circuit breaker is in the closed I (ON) position when connecting, the pre-trip mechanism trips it before the pins are connected.
Protection Against Direct Contact with Power Circuits
An adapter enables the base to take the same isolation and connection accessories as the unit-mount circuit breaker.


DANGER