Responding to a Trip
Taking Precautions Before Responding to a Trip
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Identifying the Cause of the Trip
Local and remote indication provides information on the probable cause of a trip.
The causes are of several types:
-
Faults detected on the installation
-
Faults detected due to a malfunction
-
Intentional tripping
Trip Following a Fault on the Installation
The control mechanism is positioned on
, or Trip.
|
Indication |
Probable cause |
|---|---|
|
SD |
Tripped manually by:
|
|
SD and SDE |
Tripped on electrical fault, cause unknown |
Maintenance of the Equipment Following Trip on Electrical Fault
The fact that the protection has tripped does not remedy the cause of the fault on the downstream equipment.
WARNING |
|---|
|
HAZARD OF CLOSING ON ELECTRICAL FAULT
Do not close the circuit breaker again without first inspecting
and, if necessary, repairing the downstream electrical equipment.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Isolate the feed before inspecting the electrical equipment downstream of the protection.
Perform the following tasks after a short-circuit:
-
Carefully clean off any traces of black smoke. The smoke particles can conduct electricity.
-
Check the power connections and control wires.
-
Operate the circuit breaker at least five times at zero load.
Depending on the type of fault, perform maintenance inspections on all or part of the equipment where the fault occurred:
-
Minor faults: Tripped by overload protection
Following repairs, checks E, F, and G must be carried out.
-
Serious or destructive faults:
-
Tripped due to unknown electrical fault
-
Tripped by short-circuit protection
-
Tripped by ground-fault protection
Special care must be taken to prevent double ground faults in photovoltaic applications.
Following repairs, checks A, D, E, G, and J must be carried out. Check the circuit breaker that tripped before being returned to service.
-
If restarting is a high priority (for example, a safety installation), the defective part of the installation must be isolated and locked in order to carry out this maintenance.
DANGER
WARNING