DOCA0066EN-05

Front Face Description

Front Face

A Faceplate

B Toggle handle for opening, closing, and resetting

C Push-to-trip button

D Circuit breaker rating

E Trip unit (circuit breaker only)

F Trip unit adjustment dials (circuit breaker only)

For more information about installation, refer to the instruction sheets.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?