TM-DC Thermal-Magnetic Trip Unit for 3P and 4P Circuit Breakers from 80 A to 250 A
Introduction
The TM-DC thermal-magnetic trip unit for 3P/4P circuit breakers from 80 A to 250 A are interchangeable trip units.
They are designed for DC general-purpose applications.
The TM-DC 3P/4P trip units provide:
-
adjustable thermal threshold
-
fixed magnetic pick-up on trip units with In from 80 A to 160 A
-
adjustable magnetic pick-up on trip units with In 200 A and 250 A
Description
Setting the Thermal Protection
The thermal protection pick-up Ir is set by a 4-setting dial.
The following table shows the values of the pick-up Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.
|
Trip Unit Rating In (A) at 40 °C (104 °F) |
|||||
|---|---|---|---|---|---|
|
80 |
100 |
125 |
160 |
200 |
250 |
|
Pick-up Ir (A) at 40 °C (104 °F) |
|||||
|
56 |
70 |
87 |
112 |
140 |
175 |
|
64 |
80 |
100 |
128 |
160 |
200 |
|
72 |
90 |
112 |
144 |
180 |
225 |
|
80 |
100 |
125 |
160 |
200 |
250 |
Setting the Magnetic Protection on Trip Units With In from 80 A to 160 A
For trip units rated below 200 A, the magnetic protection pick-up cannot be adjusted and equals the value shown below:
|
Trip Unit Rating In (A) |
||||
|---|---|---|---|---|
|
80 |
100 |
125 |
160 |
|
|
Fixed Pick-up Ii (A) +/– 20% |
||||
|
True DC value |
800 |
800 |
1,250 |
1,250 |
Setting the Magnetic Protection on Trip Units With In 200 A and 250 A
For trip units rated between 200 A and 250 A, the magnetic protection pick-up Ii is set by a 6-setting dial.
The following table shows the values of the pick-up Ii (in amperes) for magnetic protection (values indicated on the dial), relative to the position of the Ii dial:
|
Trip Unit Rating In (A) |
|
|---|---|
|
200 |
250 |
|
Pick-up Ii (A) +/– 20% |
|
|
1,000 |
1,250 |
|
1,200 |
1,500 |
|
1,400 |
1,750 |
|
1,600 |
2,000 |
|
1,800 |
2,250 |
|
2,000 |
2,500 |