NSX Cord
Introduction
The NSX cord connects a circuit breaker to the communication network.
The NSX cord can be used with a BSCM module.
For more information about integrating ComPact NSX DC circuit breaker communication functions, refer to:
-
DOCA0093EN ULP System (IEC Standard) – ULP (Universal Logic Plug) System – User Guide
-
DOCA0091EN ComPact NSX - Modbus Communication Guide
Description
The NSX cord consists of a junction box, a cable equipped with an RJ45 connector, and a cable equipped with a screw terminal block.

|
Item |
Data medium |
Data transmitted |
Comments |
|---|---|---|---|
|
A |
NSX cord microswitch |
State of SD contact |
The NSX cord goes into the SD slot instead of the auxiliary contact. |
|
B |
Cable equipped with an RJ45 connector for connection to a ULP module. |
Communication network |
Three cable lengths are available: 0.3 m (9.84 ft), 1.3 m (4.27 ft), and 3 m (14.7 ft). |
|
C |
Internal link to the BSCM module |
Communication network |
– |
The NSX cord also provides the 24 Vdc power supply for the BSCM module (when this module is installed):
Installation
The slots used to install the NSX cord depend on the circuit breaker type.
The NSX cord cannot be installed at the same time as the SD auxiliary contact.
The NSX cord can be installed on site.
For more information about installation, consult the instruction sheet on the Schneider Electric website: GHD16047AA ComPact NSX100–630 – NSX cord.
Communication with the NSX Cord
The NSX cord connects to the following ULP modules:
-
IFM or IFE communication interface
-
FDM121 display
-
IO module