Front Face Description
Front Face with Direct Rotary Handle
The circuit breaker operating controls, operation indicators, settings, and locking mechanisms for the direct rotary handle are on the front of the circuit breaker.
A Faceplate
B Direct rotary handle for opening, closing, and resetting
C Push-to-trip button
D Trip unit (circuit breaker only)
E Trip unit adjustment dials (circuit breaker only)
For more information about rotary handle configuration and installation, consult the instruction sheets on the Schneider Electric website:
-
GHD16291AA Direct rotary handle for ComPact NSX100-250 DC
-
GHD16319AA Direct rotary handle for ComPact NSX400-630 DC
Front Face with Extended Rotary Handle
For circuit breakers with an extended rotary handle:
-
The circuit breaker operating controls are on the door escutcheon.
-
The operation indicators and settings are only accessible when the door is open
-
The locking mechanisms are on the circuit breaker (optional) and on the door escutcheon (door closed).
There are two models of extended rotary handle:
-
Black handle for standard applications
-
Red handle on yellow bezel for machine control applications
For more information about extended rotary handle installation, consult the instruction sheets on the Schneider Electric website:
-
GHD16292AA Extended rotary handle for ComPact NSX100-250 DC
-
GHD16320AA Extended rotary handle for ComPact NSX400-630 DC
Rotary Handle and Accessories Installation Demonstration Video
The following information is available in a demonstration video:
-
Installation of a direct mounted rotary handle and accessories (for example, keylocks) on a ComPact NSX100–250 circuit breaker
-
Installation of an extended rotary handle and accessories on a ComPact NSX100–250 circuit breaker
To access the video, click the following link: https://youtu.be/h7ETxmroxiI, copy and paste the link to your Web browser, or scan the QR code.