Control Auxiliaries
Control and Indication Contacts Installed Outside the Circuit Breaker
Control and indication contacts installed outside the case are contacts for specific applications. Refer to LVPED208006EN ComPact NSX, ComPact INS/INV, MasterPact NW DC - DC PV Catalog.
|
CAM contacts |
Early-operation contacts Install in the rotary handle:
|
|
Carriage switches |
Connected (CE)/Disconnected (CD) carriage switches Install on the chassis to indicate the position of the circuit breaker in the chassis: A Connected position carriage switch (CE) B Disconnected position carriage switch (CD) |
Voltage Trip Releases
Use voltage trip releases to trip circuit breakers deliberately using an electrical signal. Install these auxiliaries in the case under the front face.
The characteristics of these auxiliaries comply with the recommendations of standard IEC/EN 60947-2.
|
MN |
MN undervoltage trip release This release:
Use this type of trip release for fail-safe emergency stops. |
|
Time-delay unit |
Time-delay unit for MN undervoltage trip release The time-delay unit eliminates nuisance tripping of an undervoltage trip release due to transient voltage dips lasting < 200 ms. There are 2 types of time-delay units: adjustable or fixed. |
|
MX |
MX shunt trip release This release trips the circuit breaker when the voltage exceeds 0.7 times the rated voltage Un. |