990-6538F-001

Connect the PBUS Cables

NOTE: Do not connect the PBUS cables to the network. The connection is not intended for network connection and may cause inoperability of the network.
  1. Connect the provided PBUS 1 (white) and PBUS 2 (red) cables to the PBUS ports on the UPSs.
  2. Mount termination plugs (T) in the unused connectors.

    Example of System with Three UPSs in Parallel without the RIM

    Example of System with Three UPSs in Parallel with the RIM

    NOTE: If the RIM is present, the PBUS cables between the two intelligence modules in one UPS (highlighted in green) should be obtained from the redundant intelligence module kit SP3OPT001.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.