990-6538F-001

Connect the Power Cables for the UPS with One Internal Switch

NOTICE
RISK OF EQUIPMENT DAMAGE
To ensure correct load sharing in bypass operation in a parallel system:
  • All bypass cables must be the same length for all UPSs.
  • All output cables must be the same length for all UPSs.
  • All input cables must be the same length for all UPSs (only required in single mains system).
Failure to follow these instructions can result in equipment damage.
  1. Only for dual mains: Remove the single mains jumper busbars.
    NOTE: Save the single mains jumper busbars. They are needed for testing during start-up of the UPS.

    Front View of the UPS

  2. Connect the power cables in the described order.
    1. Connect the PE cables.
      NOTE: The earth/PE connection must be common for all the UPSs in the parallel system.
    2. Connect the input cables (L1, L2, L3, (N)).
    3. Only for dual mains: Connect the bypass cables (L1, L2, L3, N).
    4. Connect the output cables (L1, L2, L3, N).
    5. Connect the DC cables (DC+, DC-).

    Single Mains

    Dual Mains

  3. Reinstall the rear panel on the UPS.

    Rear View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.