990-6538F-001

Install the Seismic Anchoring (Option)

NOTE: Use the optional seismic kit SP3OPT005 for this procedure.
  1. Push the UPS into the final position.
  2. Install the rear anchoring bracket on the UPS with the provided M8 x 20 bolts.

    Option: Use the shimming sheet (870-91123) for alignment with a two meter tall rack.

    Rear View (without Shimming Sheet)

    Rear View (with Shimming Sheet)

  3. Mount the rear anchoring bracket to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchors is ø14 mm. The requirement is M12 strength grade 8.8 hardware.

    Rear View (without Shimming Sheet)

    Rear View (with Shimming Sheet)

  4. Install the front anchoring bracket on the UPS and mount it to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchors is ø14 mm. The requirement is M12 strength grade 8.8 hardware.

    Option: Use the shimming sheet (870-91123) for alignment with a two meter tall rack.

    Front View (without Shimming Sheet)

    Front View (with Shimming Sheet)

    Front View (without Shimming Sheet)

    Front View (with Shimming Sheet)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.