990-6538F-001

Final Installation

  1. Reinstall the cover over the signal connection terminals.

    Front View of the UPS

  2. Reinstall the front inner cover(s) on the UPS.

    UPS with One Internal Switch

    UPS with Four Internal Switches

  3. For parallel system: Install a padlock (not provided) on the internal maintenance disconnect device IMB in the open position on all UPSs in the parallel system.
  4. Fill out the model-specific power rating information on the UPS name plate.
  5. Remove the labels 885-92827(x 2) and 885-92828 (x 1) from the top dust covers.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.