Install the Power Module(s)
WARNING |
|---|
|
RISK OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
RISK OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
Heavy load
Power modules are heavy (28 kg) and require two persons
to lift.
Failure to follow these instructions can result in injury or equipment damage.
|
- Remove the filler plate from the empty power module slot. Save the filler plate for future use.
- Set the unlock tab on the power module to the OFF position. Push the power module into the slot. The enable mechanism will latch when the power module is correctly inserted.
- Reinstall the screws in the sides of the power module.
- Set the unlock tab on the power module to the ON position.
DANGERHazard of electric shock, explosion, or arc flashAll power module slots must have either a power module or a filler plate installed.Failure to follow these instructions will result in death or serious injury.
WARNING
CAUTION