990-6538F-001

Install the Neutral Disconnection Kit (Option)

NOTE: Use the optional neutral disconnection kit SP3OPT004 for this procedure. The neutral disconnection kit is only applicable for a UPS with one internal switch.
  1. Remove the plastic cover from the neutral disconnection assembly.
  2. Install the neutral disconnection assembly to the rear posts in the UPS with the four provided screws.

    Rear View of the UPS

  3. Connect the bottom busbar of the neutral disconnection assembly to the neutral busbar in the UPS with the two provided screws.

    Front View of the UPS

  4. Connect the external neutral cables to the upper busbar of the neutral disconnection assembly.

    Rear View of the UPS

  5. Reinstall the plastic cover on the neutral disconnection assembly.

    Rear View of the UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.