990-6538F-001

Installation Procedure

DANGER
Hazard of electric shock, explosion, or arc flash
The UPS must be secured against movement. Perform one of the following actions/procedures once the UPS is in its final position:
  • Reinstall the front transportation bracket on the UPS and mount it to the floor, OR
  • Install the seismic anchoring kit.
Failure to follow these instructions will result in death or serious injury.
WARNING
TILTING HAZARD
The cabinet is top heavy - move with care and use ramps over uneven floors.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Perform one of the following procedures:
  2. Perform one of the following procedures:
  3. Only for TN-C earthing system: Prepare for TN-C Earthing System.
  4. Only for UPS with one internal switch: Install the Neutral Disconnection Kit (Option).
  5. Perform one of the following procedures:
  6. Connect the Signal Cables.
  7. Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products.
  8. Connect the Modbus Cables.
  9. Only for parallel system: Connect the PBUS Cables.
  10. Install the Power Module(s).
  11. Install the Redundant Intelligence Module (RIM) Kit (Option).
  12. Final Installation.
For moving or decommissioning the UPS after installation has been completed, see Decommission or Move the UPS to a New Location.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.