990-6538F-001

Install the Redundant Intelligence Module (RIM) Kit (Option)

NOTE: Use the optional redundant intelligence module (RIM) kit SP3OPT001 for this procedure.
  1. Remove the IM2 slot cover.
  2. Loosen the indicated screw and remove the enable switch fixing plate. Set the enable switch to the OFF position.
  3. Install the redundant intelligence module from the kit in the slot with two screws.
    NOTE: Push on the bottom part of the intelligence module to ensure a smooth push-in.
  4. Set the enable switch to the ON position. Reinstall the enable switch fixing plate and fasten with the screw removed in step 2.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.