Decommission or Move the UPS to a New Location
- Shut down the UPS completely – follow the instructions in the UPS operation manual.
- Lockout/Tagout all disconnect devices in the maintenance bypass panel/the switchgear in the OFF (open) position.
- Lockout/Tagout all battery disconnect devices in the switchgear/battery solution in the OFF (open) position.
- Open the front door of the UPS.
- Remove all the power modules EXCEPT the power module in the lowest position. See Install the Power Module(s) for details.
- Remove the front inner cover(s) from the UPS.
- Measure for and verify ABSENCE of voltage on each measurement
point before continuing.
DANGERhAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHMeasure for and verify ABSENCE of voltage on each measurement point before continuing.Failure to follow these instructions will result in death or serious injury.Number Description Number Description 1 Output L3 7 Battery + 2 Output L2 8 Battery – 3 Output L1 9 Neutral 4 Bypass L3 10 Input L3 5 Bypass L2 11 Input L2 6 Bypass L1 12 Input L1 Number Description Number Description 1 UIB L1 (in) 18 SSIB L3 (in) 2 UIB L2 (in) 19 SSIB N (out) 3 UIB L3 (in) 20 SSIB L1 (out) 4 UIB L1 (out) 21 SSIB L2 (out) 5 UIB L2 (out) 22 SSIB L3 (out) 6 UIB L3 (out) 23 UOB N (out) 7 MBB N (in) 24 UOB L1 (out) 8 MBB L1 (in) 25 UOB L2 (out) 9 MBB L2 (in) 26 UOB L3 (out) 10 MBB L3 (in) 27 UOB N (in) 11 MBB N (out) 28 UOB L1 (in) 12 MBB L1 (out) 29 UOB L2 (in) 13 MBB L2 (out) 30 UOB L3 (in) 14 MBB L3 (out) 31 Battery + 15 SSIB N (in) 32 Battery – 16 SSIB L1 (in) 33 Battery N 17 SSIB L2 (in) - Measure for and verify ABSENCE of voltage on each input/bypass/output/DC busbar before continuing.
- Disconnect and remove all power cables from the UPS. See Connect the Power Cables for the UPS with One Internal Switch or Connect the Power Cables for the UPS with Four Internal Switches for details.
- Reinstall the front inner cover(s) and reinstall the screws.
- Remove the cover from the signal connection terminals.
- Disconnect and remove all signal cables from the UPS. See Connect the Signal Cables for details.
- For UPS system with a depth adapter: Remove the interconnection hardware between the UPS and the depth adapter. Remove the depth adapter. See the installation manual provided with the depth adapter for details. Save all parts for reinstallation.
- For UPS system with a bottom entry cabinet: Remove the interconnection hardware between the UPS and the bottom entry cabinet. Remove the bottom entry cabinet. See the installation manual provided with the bottom entry cabinet for details. Save all parts for reinstallation.
- Reinstall all removed plates and covers. See Final Installation for details.
- If present, remove the front seismic anchoring bracket/front transportation bracket from the UPS and the floor. Save for reinstallation.
- If present, remove the rear seismic anchoring bracket/rear transportation bracket from the UPS and from the floor. Save for reinstallation.
- Close and lock the front door.
- Raise the feet of the UPS until the casters have full contact with the floor.
- You can now move the UPS by rolling it over the floor on
the casters.
WARNINGTIPPING hazard- The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
- The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
- Move at a slow pace and pay close attention on the floor conditions and the balance of the UPS.
Failure to follow these instructions can result in death, serious injury, or equipment damage. - For transport over longer distances or
in conditions that are not suitable for the casters of the UPS:
WARNINGTop-heavy cabinetThe UPS will be top-heavy with one power module installed. Take appropriate precautions during handling and preparation for transport/shipment.Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNINGTIPPING hazardFor transport over longer distances or in conditions that are not suitable for the casters of the UPS, ensure:- that personnel performing the transport have necessary skill and have received adequate training;
- to use appropriate tools to safely lift and transport the UPS;
- to protect the product against damage by using appropriate protection (like wrapping or packaging).
Failure to follow these instructions can result in death, serious injury, or equipment damage.Transportation requirements:
-
Schneider Electric recommends to reuse the original shipping pallet in combination with the original transportation brackets for long-distance transportation, if in undamaged condition. If the original shipping pallet and original transportation brackets are not available or are damaged, use an appropriate pallet suitable for the weight of the UPS (309 kg with one power module installed) with appropriate dimensions (minimum 1250 mm x 900 mm).
-
Use appropriate means of fixation to mount the UPS to the pallet. Follow the procedures in the receiving and unpacking manual to fix the UPS to the pallet when using the original pallet and transportation brackets.
DANGERTIPPING hazard- The UPS must be appropriately fixed to the pallet immediately after being placed on the pallet.
- The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
Failure to follow these instructions will result in death or serious injury.
WARNINGUnexpected equipment behaviorDo not lift the UPS with a forklift/pallet truck directly on the frame as it may bend or damage the frame.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Perform one of the following:
- Decommission the UPS, OR
- Move the UPS to a new location to install it.
- Only for installing the UPS in a new location: Follow
the installation manual to install the UPS in the new location. See Installation Procedure for installation overview.
Start-up must only be performed by Schneider Electric.
DANGERhAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHStart-up must only be performed by Schneider Electric.Failure to follow these instructions will result in death or serious injury.
CAUTION