990-6538F-001

Position the UPS

DANGER
Hazard of electric shock, explosion, or arc flash
The UPS must be secured against movement. Once the UPS is in its final position, reinstall the front and rear transportation brackets on the UPS and mount them to the floor.
Failure to follow these instructions will result in death or serious injury.
  1. Push the UPS into the final position.
  2. Lower the front and rear feet on the UPS with a wrench until they connect with the floor. The casters must not have contact with the floor. Use a bubble-leveler to check that the UPS is level.
  3. Reinstall the front transportation bracket on the UPS and mount it to the floor. Use appropriate hardware for the floor type – the hole diameter in the bracket is ø10 mm. The requirement is M8 strength grade 8.8 hardware.
  4. Reinstall the rear transportation bracket on the UPS and mount it to the floor. Use appropriate hardware for the floor type – the hole diameter in the bracket is ø10 mm. The requirement is M8 strength grade 8.8 hardware.

    Rear View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.