990-6538F-001

Parallel System Overview

The UPS can support up to 4 UPSs in parallel for capacity and up to 3+1 UPSs in parallel for redundancy.

NOTE: In a parallel system, an external maintenance bypass disconnect device (Ext. MBB) must be provided and the internal maintenance disconnect device IMB and MBB (marked with an * in the diagrams) must be padlocked in the open position.

UPS with One Internal Switch

UIB Unit input disconnect device
SSIB Static switch input disconnect device
UOB Unit output disconnect device
SIB System isolation disconnect device
BB Battery disconnect device
IMB Internal maintenance disconnect device
Ext. MBB External maintenance bypass disconnect device
NOTE: In Schneider Electric literature, 'disconnect device' is used as a generic term covering circuit breakers or switches as their position may vary depending on configuration. Details about the individual configuration are found in the electrical diagram and/or by reading the symbol on the front of each disconnect device.

Parallel System – Single Mains (One Internal
Switch)

Parallel System – Dual Mains (One Internal
Switch)

UPS with Four Internal Switches

UIB Unit input disconnect device
SSIB Static switch input disconnect device
UOB Unit output disconnect device
SIB System isolation disconnect device
BIB Bypass input disconnect device
MIB Main input disconnect device
BB Battery disconnect device
MBB Maintenance bypass disconnect device
Ext. MBB External maintenance bypass disconnect device
NOTE: In Schneider Electric literature, 'disconnect device' is used as a generic term covering circuit breakers or switches as their position may vary depending on configuration. Details about the individual configuration are found in the electrical diagram and/or by reading the symbol on the front of each disconnect device.

The UPS can support up to 4 UPSs in parallel for capacity and up to 3+1 UPSs in parallel for redundancy.

Parallel System – Single Mains (Four Internal Switches)

Parallel System – Dual Mains (Four Internal Switches)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.