990-6538F-001

Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.
  1. Install the optional battery temperature sensor in the battery solution. In battery cabinets, install the battery temperature sensor in the top corner of the battery cabinet.
    WARNING
    Hazard of fire
    Position the battery temperature sensor as described to ensure correct temperature measurements.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  2. Route the battery temperature sensor cables from the battery solution to the UPS and connect as shown.
    NOTE: Battery temperature sensors (SP3OPT006) are available as an optional kit.
    NOTE: The battery temperature sensor cables are considered Class 2/SELV. Class 2/SELV circuits must be isolated from the primary circuitry.
  3. Connect the signal cables from the battery disconnect device(s) in your battery solution for shunt trip or undervoltage (UV) trip connection to the UPS. Follow the illustration for connection with internal 24 VDC supply. The UPS can connect to and monitor up to three (if J8301-10 is used for backfeed) or four battery disconnect devices.
    1. Connect battery disconnect device 1 to terminal J8301 in the UPS.
    2. Connect battery disconnect device 2 to terminal J8301 in the UPS.
    3. Connect battery disconnect device 3 to terminal J8301 in the UPS.
    4. Connect battery disconnect device 4 to terminal J8301 in the UPS.
    5. For battery disconnect device trip 4, connect trip unit negative to pin 1 or 4 or 7 of terminal J8301.
    NOTE: The following diagram and table demonstrate the battery disconnect device trip connection with internal 24 VDC supply and pin connections.

    Battery Disconnect Device Trip Connection with Internal 24 VDC Supply

    J8301 Pin Connections for Battery Disconnect Device(s)

    The cable supplying the shunt trip shall be a jacket cable and rated for 600 VAC. The cables shall be sized taking the cable voltage drop and the recommendation of the shunt trip manufacturer into consideration.

    Battery Disconnect Device 1

    Pin number Function
    1 GND
    2 BB_UV_TRIP_1
    3 BB_SHUNT_TRIP_1

    Battery Disconnect Device 2

    Pin number Function
    4 GND
    5 BB_UV_TRIP_2
    6 BB_SHUNT_TRIP_2

    Battery Disconnect Device 3

    Pin number Function
    7 GND
    8 BB_UV_TRIP_3
    9 BB_SHUNT_TRIP_3

    Battery Disconnect Device 4

    Pin number Function
    10 24 V
    11 BB_UV_TRIP_4
    12 BB_SHUNT_TRIP_4
  4. Connect signal cables from the auxiliary contacts in your switchgear to the UPS.
    Terminal number Function Connection
    J8302, 1-2 UIB (unit input disconnect device) Connect to normally open (NO) auxiliary contacts in unit input disconnect device UIB. UIB must contain an auxiliary contact for each connected UPS.
    J8302, 3-4 SSIB (static switch input disconnect device) Connect to normally open (NO) auxiliary contacts in static switch input disconnect device SSIB. SSIB must contain an auxiliary contact for each connected UPS.
    J8302, 5-6 Ext. MBB (external maintenance bypass disconnect device) Connect to normally closed (NC) auxiliary contacts in external maintenance bypass disconnect device (Ext. MBB). Ext. MBB must contain an auxiliary contact for each connected UPS.
    J8302, 7-8 UOB (unit output disconnect device) Connect to normally open (NO) auxiliary contacts in unit output disconnect device UOB.
    J8303, 1-2 RUOB (redundant AUX switch in unit output disconnect device) Connect to redundant auxiliary contacts in unit output disconnect device UOB.
    J8303, 3-4 SIB (system isolation disconnect device) Connect to normally open (NO) auxiliary contacts in system isolation disconnect device SIB for parallel system. SIB must contain an auxiliary contact for each connected UPS.
    J8304, 1-2 BB1 (battery disconnect device 1) Connect to normally open (NO) auxiliary contacts in battery disconnect device number 1.
    J8304, 3-4 BB2 (battery disconnect device 2) Connect to normally open (NO) auxiliary contacts in battery disconnect device number 2.
    J8304, 5-6 BB3 (battery disconnect device 3) Connect to normally open (NO) auxiliary contacts in battery disconnect device number 3.
    J8304, 7-8 BB4 (battery disconnect device 4) Connect to normally open (NO) auxiliary contacts in battery disconnect device number 4.
    J8305, 1-2 One internal switch UPS:
    IMB (internal maintenance disconnect device)
    Four internal switches UPS:
    MBB (maintenance bypass disconnect device)
    Connect to normally closed (NC) auxiliary contacts in internal maintenance disconnect device IMB or maintenance bypass disconnect device MBB.
    J8310, 1 Backfeed relay common See Backfeed Protection.
    J8310, 2 Backfeed relay normally closed (NC) See Backfeed Protection.
    J8310, 3 Backfeed relay normally open (NO) See Backfeed Protection.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.