990-91580E-001

EPO

EPO Configurations on Board 640-02383 (Terminal J6600, 1-9)

The EPO input supports 24V SELV.

NOTE: The default setting for the EPO activation is to turn off the inverter.

If you want the EPO activation to transfer the UPS into forced static bypass operation instead, please contact Schneider Electric.

For more information about terminal locations, see Signal Connection Terminals.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.