990-91580E-001

Configuration Options

  • Compact design, high density technology, and modular architecture

  • Replacement of power module in any operation mode (Live Swap)*

  • Single or dual mains

  • Default top cable entry. Bottom cable entry available with bottom entry cabinet or depth adapter installed.

  • ECO mode

  • EcoStruxure IT compatible

  • Redundant intelligence controller

  • Redundant network management card

  • Generator compatible

  • Power module flexible derating

  • Up to 4+0 UPSs in parallel for capacity

  • Up to 3+1 UPSs in parallel for redundancy

  • Lithium battery compatibility

  • Common battery in parallel system

  • Touchscreen LCD

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.