990-91580E-001

Signal Connection Terminals

Overview of Signal Connection Terminals in the UPS

  1. Remote EPO (J6600)

  2. Display port (for internal use)

  3. USB port (for service)

  4. Tuner port (for service)

  5. Modbus port

  6. Battery temperature sensor (J3008)

  7. Input contacts (J3009)

  8. Output relays (J3001)

  9. PBUS2

  10. PBUS1

  11. Network management card (NMC) slot 1

  12. Network management card (NMC) slot 2

  13. Backfeed relay and sync output relay (J8310)

  14. Auxiliary contacts 1 (J8302)

  15. Auxiliary contacts 2 (J8303)

  16. Battery disconnect device auxiliary contacts (J8304)

  17. IMB and RIMB auxiliary contacts (J8305)

  18. Sync input (J8300)

  19. Battery disconnect device trip (J8301)

  20. IM1 slot for intelligence module

  21. IM2 slot for intelligence module

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables (A to L) separately from the non-Class 2/non-SELV cables (M to S). Non-Class 2/non-SELV cables should be rated for 600 V.
NOTE: The recommended size for the signal cables is 0.5 mm2.
NOTE: Do not unplug the signal terminals by hand. Be sure to use the tool (TME12560) in the accessory bag to unplug the signal terminals. Be sure to restore the two rows of terminals to their original position: the grey terminals in the upper row and the green terminals in the lower row.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.