990-91580E-001

Configurable Input Contacts and Output Relays

Input Contacts

Four input contacts are available and can be configured to indicate a given event via the display.

The input contacts support 24 VDC 10 mA. All circuits connected must have the same 0 V reference.

Name Description Location on board 640-02383
IN _1 (input contact 1) Configurable input contact Terminal J3009, 1-2
IN _2 (input contact 2) Terminal J3009, 3-4
IN _3 (input contact 3) Terminal J3009, 5-6
IN _4 (input contact 4) Terminal J3009, 7-8

Output Relays

Five output relays are available and can be configured to activate on one or more events via the display.

The output relays support 24 VAC/VDC 1 A. All external circuitry must be fused with maximum 1 A fast acting fuses.

Name Description Location on board 640-02383
OUT _1 (output relay 1) Configurable output relay Terminal J3001, 1 (Comm), 9 (NO), 2 (NC)
OUT _2 (output relay 2) Terminal J3001, 10 (Comm), 3 (NO), 11 (NC)
OUT _3 (output relay 3) Terminal J3001, 4 (Comm), 12 (NO), 5 (NC)
OUT _4 (output relay 4) Terminal J3001, 13 (Comm), 6 (NO), 14 (NC)
OUT _5 (output relay 5) Terminal J3001, 7 (Comm), 15 (NO), 8 (NC)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.