990-91580E-001

Communication and Management

Local area network 1 Gbps – 1 port as default
Modbus Modbus (SCADA)
Output relays 5 x SELV configurable
Input contacts 4 x SELV configurable
Standard control panel 7 inch touchscreen display
Audible alarm Yes
Emergency Power Off (EPO) Options:
  • Normally Closed (NC) with 24 VDC external supply

  • Normally Open (NO) with 24 VDC external supply

  • Normally Closed (NC)/Normally Open (NO)

  • Normally Open (NO)

  • Normally Closed (NC)

External switchgear For UPS with one internal switch:
UIB
UOB
SSIB
Ext. MBB
SIB
BB
For UPS with four internal switches:
Ext. MBB
SIB
BB
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.