990-91580E-001

Inverter Short Circuit Current

Term Explanations

IK1 Short circuit between a phase and neutral
IK2 Short circuit between two phases
IK3 Short circuit between three phases

S [kW]

IK1 IK2 IK3

50

182 A/220 ms

172 A/220 ms

161 A/220 ms

100

364 A/220 ms

344 A/220 ms

322 A/220 ms

150

546 A/220 ms

516 A/220 ms

483 A/220 ms

200

728 A/220 ms

688 A/220 ms

644 A/220 ms

250

904 A/220 ms

862 A/220 ms

807 A/220 ms

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.