990-91580E-001

Derating Due to Load Power Factor

0.7 leading to 0.7 lagging without derating.

UPS rating UPS output
Lagging Leading
PF=1 PF=0.7 PF=0.8 PF=0.9 PF=0.9 PF=0.8 PF=0.7
100 kVA/kW

100 kVA/70 kW

100 kVA/80 kW

100 kVA/90 kW

100 kVA/90 kW

100 kVA/80 kW

100 kVA/70 kW

150 kVA/kW

150 kVA/105 kW

150 kVA/120 kW

150 kVA/135 kW

150 kVA/135 kW

150 kVA/120 kW

150 kVA/105 kW

200 kVA/kW

200 kVA/140 kW

200 kVA/160 kW

200 kVA/180 kW

200 kVA/180 kW

200 kVA/160 kW

200 kVA/140 kW

250 kVA/kW

250 kVA/175 kW

250 kVA/200 kW

250 kVA/225 kW

250 kVA/225 kW

250 kVA/200 kW

250 kVA/175 kW

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.