990-91079J-001

Set the Life Cycle Monitoring

NOTICE
risk of equipment damage
Only trained personnel following the required training course may undertake modifications to UPS system parameters.
Failure to follow these instructions can result in equipment damage.
  1. On the display, select and then select LCM Set.
  2. You now have the following options:
    • Select Set dust filter expiration to set the service life of the dust filter.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.