990-91079J-001

Replace the Dust Filter

  1. Lift the front panel free of the UPS cabinet.
    NOTE: Be careful not to disconnect the cable on the rear side of the front panel.
  2. Loosen the screws and remove the metal brackets and the manual box..

    UPS for External Batteries

    UPS with Internal Batteries

  3. Replace the dust filter.

    UPS for External Batteries

    UPS with Internal Batteries

  4. Reinstall the metal brackets and fasten with the screws.
  5. Reinstall the front panel.
  6. Reset the dust filter time in the display. See Set the Life Cycle Monitoring for more information.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.