990-91079J-001

Transfer a Parallel System from Normal Mode to Maintenance Bypass Mode

  1. On all UPS displays, select and then select Function > To bypass.

    The parallel system will transfer to static bypass mode.

  2. Turn the external maintenance bypass breaker Ext. MBB to the ON (closed) position.

    The load is now supplied via the external maintenance bypass breaker.

  3. Turn the battery breakers BB of all UPSs to the OFF (open) position.
  4. Disconnect the battery relay from the display by selecting the battery symbol and selecting Batt relay control ON/OFF and confirm to turn off the battery relay. Verify that the Relay status is now off.
  5. Open external battery breaker if external batteries are connected.
  6. Turn the mains input breakers MIB and the bypass input breakers BIB of all UPSs to the OFF (open) position.
  7. Turn the system isolation breaker SIB to OFF (open) position.
  8. For the UPS with internal batteries, disconnect all batteries on the front of the UPS.
    DANGER
    hazard of electrical shock, explosion or arc flash
    • Wait at least 5 minutes before removing the cover of the UPS after the display has turned off to allow for the capacitors to fully discharged.
    • Always measure for hazardous voltages on all terminals before working on the UPS.
    Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.