990-91079J-001

Start Up a Single UPS in Normal Mode

NOTE: When the UPS starts, the stored settings will be used.
NOTE: The log can be accessed during start-up.
  1. Check that all breakers are in the OFF (open) position.
  2. Turn the static switch input breaker SSIB to the ON (closed) position.

    The display turns on and the Home screen is shown.

  3. Turn the unit output breaker UOB to the ON (closed) position.

    Wait approximately 2030 seconds until the bypass and output LEDs turn green. The UPS starts up in static bypass mode.

  4. Turn the unit input breaker UIB to the ON (closed) position.

    The rectifier ramps up and the LEDs on the user interface show as follows:

  5. When the rectifier LED turns steady green, the inverter synchronizes with bypass.

    The LEDs on the user interface show as follows:

  6. Wait approximately one minute until the inverter LED turns steady green, the UPS transfers automatically from static bypass mode to normal mode.

    The LEDs on the user interface show as follows:

  7. Turn the battery breaker(s) BB to the ON (closed) position.

    The LEDs on the user interface show as follows:

    The UPS is now in normal mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.