990-91079J-001

Transfer a Single UPS from Static Bypass Mode to Normal Mode

NOTE: The UPS will normally transfer automatically from static bypass to normal mode. This procedure can be used to manually transfer to normal mode if the bypass frequency is above the specified limits.
  1. On the display, select and then select ESC bypass.

    The LEDs on the user interface show as follows:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.