990-91079J-001

User Interface

Keys

Home Previous Next Confirm

EPO

Only use the EPO button in case of emergency.

It can be configured whether, when the EPO is activated, the UPS should:

  • turn off the rectifier, inverter, charger, and static bypass and stop supplying the load immediately (default), or

  • transfer to static bypass mode and continue supplying the load.

DANGER
hazard of electric shock, explosion, or arc flash
The UPS control circuit will remain active after the EPO has been pushed if utility/mains is available.
Failure to follow these instructions will result in death or serious injury.

Status LEDs

  LED Status
A Rectifier

Green : Rectifier is working correctly.

Flashing green : Rectifier is starting up.

Red : Rectifier is inoperable.

Flashing red : Utility/mains is unavailable.

OFF : Rectifier is off.

B Battery

Green : Battery is charging.

Flashing green : Battery is discharging.

Red : Battery is inoperable.

Flashing red : Battery low voltage.

OFF : Battery and battery charger are OK, battery is not charging or discharging.

C Bypass

Green : Load supplied by bypass source.

Red : Bypass source is unavailable or static bypass switch is inoperable.

Flashing red : Bypass voltage is out of tolerance.

OFF : Bypass source is OK.

D Inverter

Green : Load supplied by inverter.

Flashing green : Inverter on, start, synchronization or standby (ECO mode).

Red : Load not supplied by inverter, inverter is inoperable.

Flashing red : Load supplied by inverter, but an inverter alarm is present.

OFF : Inverter is off.

E Load

Green : UPS output is on.

Red : Overload on UPS output for too long, or output has shorted, or no output power present.

Flashing red : Overload on UPS output.

OFF : UPS output is off.

F Status

Green : UPS is OK.

Red : Inoperable status.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.