990-91079J-001

Start-Up Checklist – Only Applicable to Single UPSs with Internal Batteries

DANGER
hazard of electric shock, explosion, or arc flash
Parallel systems and UPSs for external batteries must only be started up by Schneider Electric.
Failure to follow these instructions will result in death or serious injury.
  • I have positioned the UPS according to the installation manual and the recommended clearances are respected.

  • I have verified that the environmental conditions including temperature, humidity, and airflow stated in the installation manual are respected.

  • I have verified that the input voltage and frequency are within the tolerances specified in the installation manual.

  • I have verified that the upstream protection is in accordance with the recommendations in the installation manual and that the power cables have been connected correctly.

  • I have installed the batteries as specified in the installation manual.

  • I have followed the Initial Start-Up of the UPS Using the Wizard – Only Applicable to Single UPSs with Internal Batteries.

  • I have made all settings (including battery settings and life cycle monitoring) described in this manual.

  • I have completed all functional tests successfully (normal mode, battery mode, and static bypass mode).

  • I have successfully entered the UPS passcode provided by Schneider Electric.

  • I confirm the installation has been completed and the UPS is running in normal mode and is powering the load.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.