990-91079J-001

Initial Start-Up of the UPS Using the Wizard – Only Applicable to Single UPSs with Internal Batteries

DANGER
hazard of electric shock, explosion, or arc flash
Parallel systems and UPSs for external batteries must only be started up by Schneider Electric.
Failure to follow these instructions will result in death or serious injury.

Before starting up the UPS, confirm that:

  • The room temperature is between 0 °C to 40 °C

  • The UPS has been installed according to the specified clearance dimensions.

  1. Turn the unit input breaker UIB to the ON (closed) position.
    The display turns on.
  2. Select to register the UPS or select Skip to continue. See Register Your Easy UPS 3S for more information.
  3. When the Change language prompt appears, do one of the following:
    • Select Yes and select the preferred language using the navigation keys. Select Yes again to confirm.
    • Select No to keep the current selection.
  4. When the Change voltage prompt appears, do one of the following:
    • Select Yes and select the preferred voltage using the navigation keys. Select Yes again to confirm.
    • Select No to keep the current selection.
  5. When the Change freq. prompt appears, do one of the following:
    • Select Yes and select the preferred output frequency using the navigation keys. Select Yes again to confirm.
    • Select No to keep the current selection.
  6. When the Change mode prompt appears, do one of the following:
    • Select Yes and select Normal mode, Parallel mode, or Frequency converter mode using the navigation keys. Select Yes again to confirm.
    • Select No to keep the current selection.
  7. When the Change Batt setting prompt appears, perform the following steps:
    1. Enter password: Enter the password 2334.
    2. Batt number: For IEC regions that utilize a voltage of 208 V: Verify the number of battery blocks is 20; For IEC regions that utilize a voltage of 400 V: Verify the number of battery blocks is 40.
    3. Batt cap (AH): Set the battery capacity to according to your battery configuration.
    4. Batt charge %: Set the battery charge percentage (between 1% and 15%).
    5. Select Yes to save the battery settings.
  8. When the Save new settings prompt appears, select Yes.
  9. When the Disable wizard prompt appears, do one of the following:
    • Select Yes to disable the wizard and go to the default screen.
      NOTE: Schneider Electric recommends to disable the wizard to allow for automatic start.
    • Select No to go to the default screen without disabling the wizard.
For systems with internal batteries, go to Set the Battery Settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.